StringFunctions.Soundex function

Returns the Soundex code for a string expression

Format

SQL Format:

SOUNDEX( expression )

ODBC Format:

{{ FN SOUNDEX( expression ) }}

Remarks

The scalar function SOUNDEX returns the soundex code for a string. The soundex code consists of a letter followed by three digits that provides an approximate phonetic representation of the string. This function is useful when finding names or words similar to other names or words.

Example:

The following example would return users with the name 'Steven', 'Stefan', 'Stephan' or other phonetic equivalents:

SELECT Name FROM CDBUser WHERE SOUNDEX(NAME) = SOUNDEX('Steven')


Disclaimer

Geo SCADA Expert 2021